Limiting Voltages
Image Source:
Oasishifi/Shutterstock.com
By Marcel Consée, Mouser Electronics
Published October 8, 2021
Each resistor’s purpose is to
lay obstacles in the way of electrons passing through them. This is, so the designer has control over the
currents and voltages running through the circuit. There are different ways to do that. Traditional carbon
resistors, for example, make use of differently-sized particles pressed to varying densities. This method has
large manufacturing tolerances and induces high noise levels into electronic circuits.
Carbon
composition resistors and metal foil
resistors have much better noise levels and smaller tolerances. Due to their temperature stability and
precision, metal foil resistors are the products of choice in today’s electrical and electronic
engineering.
Symbols, Colors, and the E-Series
There are two circuit symbols for resistors. Like the preference for imperial units, the US prefers a zigzag line
(Figure 1b), while the rest of the world has standardized on the rectangle as the resistor
symbol (Figure 1a). However, there is only one colour code (Figure 1c) that
indicates the Ohm value with coloured rings on conventional resistors. There can be three, four, five, or six
rings, indicating (from left to right): Value, multiplier, tolerance, and temperature coefficients.
Mouser’s Colour
Code Calculator helps to decipher the rings.
Figure 1: (a) IEC symbol, (b) ANSI symbol, (c) example of colour rings.
(Source: Mouser.com)
SMD resistors show the values more directly but still not very intuitively. For example, the letter
“R” stands for Ohm, but also stands for decimal point (examples: 7R50 = 7.5Ω; R500 =
0.5Ω Then there are the orders of magnitude: “10k” are “10kΩ”, “1M5”
are “1.5MΩ” and “0k5” “0.5kΩ”.
Figure 2: SMD resistor with 0.5Ω markings. (Source: Mouser.com)
To ensure you are using the correct resistor, it helps to measure the device using a handheld instrument like an
Ohmmeter
or a Multimeter.
Since it doesn’t make sense to manufacture resistors of every possible value, the industry invented the
‘E-Series’ of standardized values for resistors, capacitors, inductors, and Zener diodes. These
values can be combined to create virtually any required value while minimizing the number of manufactured and
stocked values. E-series resistors follow a mathematical formula determined by the n-th root:
where Vn is the rounded value, m is an integer of the E series
group size, and
n is an integer of {0, 1, 2, ..., m-1}. Manufacturers use E-series tables to provide resistors
with
standardized values and precision.
Logic combinations
When faced with a design that requires a particular resistance value that’s not readily available, there
are various options for reaching this value. One method is to use a trim potentiometer that
allows the user to adjust the resistance.
Another method is a series connection. Connecting resistors in a series, the total resistance is the sum of the
individual resistance values. This is also the principle of the voltage divider, as used in multimeters.
Connecting resistors in parallel leads to a total resistance smaller than the smallest individual resistor. The
total resistance follows the function:
Light and Heat
Light-dependent resistors (Photoresistors) provide variable resistance. They are not as sensitive as
phototransistors or photodiodes, but they are suitable for applications like analogue light dimmers. Their
resistance is reciprocally proportional to the light intensity.
Temperature-dependent resistors (Thermistors) are
another kind of resistor with variable resistance. They can be of the NTC type
(negative temperature coefficient) or the PTC type
(positive TC). The resistance of a PTC thermistor is proportional to the temperature, while it is reciprocal
with NTCs. Both types are commonly used as temperature sensors.
Conclusion
There is a wide variety of resistor types, and it should be easy to find the right one for each electronic
design. While the historic conventions regarding denomination and marking may be hard to understand, many online
tools are available that simplify the selection.
Author Bio
As Technical
Content
Specialist, Marcel is the internal contact person for technical questions in Mouser’s EMEA marketing team.
Originally a physicist, he used to work as editor for special-interest magazines in electronics. In real life,
he’s juggling two kids with too many chromosomes, a penchant for electronic gadgets and a fondness of books and
beer. Until now, none has dropped.