Honduras - Marcar Honduras

Confirme su elección de moneda:

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Smarter Industrial Control Panels with Siemens ET200SP Siemens

(Source: SIEMENS AG/W.Geyer)

Industrial control panel designers and operators commonly face challenges and requirements dealing with space constraints, a need for network connectivity, and pressure to meet environmental standards. As such, they're looking for modular designs that allow them to expand without breaking the budget, as well as improved power efficiency to meet sustainability targets and comply with regulations. Engineers also want systems that work with what they already have installed, grow as needed, and are easy to maintain.

Picture the following scenario: The production line is mid-cycle when a sensor input faults. The line stops. A supervisor watches overall equipment effectiveness (OEE) drop while a technician locates a laptop, finds the right cable, connects to the programmable logic controller (PLC), and navigates diagnostic menus to identify which of 64 channels failed. What should be a two-minute fix stretches into fifteen minutes. This is a scenario factory operators know all too well.

We sat down with Raj Rajendra, Product Manager at Siemens, to discuss how the SIMATIC ET200SP distributed I/O system changes this outcome and helps engineers overcome the challenges of control panel design. With the ET200SP's modular design, faults appear at the channel level—on LED indicators that pinpoint exactly which input or output failed. The technician reads the LED, isolates the problem to a specific module, and hot-swaps the module without interrupting the PLC or rewiring, turning a potential stop into a brief pause.

Raj Rajendra is a Product Consultant and Manager at Siemens, where he helps drive innovation and efficiency. He earned a Master’s in Industrial Systems from the Asian Institute of Technology and a Master’s in Finance from Macquarie University.

What's Driving Panel Design Now

Control panel strategy is shifting from big, centralized rooms to compact enclosures mounted near machines—where every millimeter and minute of downtime matters. As Siemens product manager Raj Rajendra explains, "In the early days, control panels were large, centralized enclosures. Over time, panels became smaller and distributed, sitting closer to machines. Today, space is at a premium, so panels need to be compact, dust-protected, and energy efficient."

Engineers want the same things: simple installation, quick fixes, and flexible connectivity, but they’re not the only ones looking to implement these features. "Electricians also want easier installation and faster troubleshooting, which is why tool-free wiring and modular expansion are so valuable," Rajendra notes. And because original equipment manufacturers (OEMs) serve mixed environments, "customers expect support for popular fieldbus systems like PROFINET and Ethernet/IP, as well as options to expand for specialized devices mounted directly on machines."

In parallel, operational data must reach the information technology (IT) layer without disrupting control operations. "Many customers now require operational data to be transmitted to the IT layer for visibility, without interfering with plant control systems," Rajendra says. "Stations must handle multiple communication standards while still supporting consistent programming and integration."

Design Once, Adapt Many Times

Frequent customer-specific changes can force redraws of electrical and mechanical files—unless the baseline is built for reuse. As Rajendra details, "Designers don't want to rework electrical and mechanical drawings every time a customer requests a different setup. Standardizing on a modular I/O platform solves that. It allows machine builders to reuse the same design and simply enable or disable modules as needed."

The benefits extend beyond design. "With our [Siemens] software tools, operators can check and document a panel without needing a PLC or programmer on-site," Rajendra explains. "Companies get to save time, energy, and money."

Inside the ET200SP

At the station level, the Siemens SIMATIC ET200SP keeps a familiar architecture—a head (interface) module with stacked I/O—but differentiates on breadth and fit. Rajendra elaborates on this point: "[Siemens] offer[s] various interface modules to cater to customer needs. A basic module is low-cost and supports fewer I/Os, while standard and high-feature modules expand to 64 I/Os, enable hot swapping, and provide richer diagnostics. Higher-tier options even let customers choose between copper or fiber optic network connections so that OEMs can match budget and performance requirements."

That flexibility addresses cabinet constraints directly. The ET200SP is 50 percent narrower than competitive devices—meaning more I/O in a smaller footprint and less spatial pressure on machine-side installations. As Rajendra puts it, "Space is one of the most valuable resources in modern plants. Narrower modules allow more I/O points to fit into a smaller cabinet, which saves huge on real estate and installation costs."

The platform extends beyond basic I/O cards. "The ecosystem is broad," Rajendra says. "We offer technology modules, communication modules, weighing modules for process industries, motor starters, RFID systems, and even small drives for stepper and servo control." For engineering teams, that breadth means a single family can reach from discrete measurement to motion and identification, which is useful when you need to add capability without redefining the platform or retraining crews.

From Fault to Fix—Faster

Fast repair requires seeing the fault where it lives, not ten clicks away. Rajendra sheds light on how Siemens helps electricians achieve this: "We built diagnostics at the channel level. For example, a 16-channel module has 16 LEDs and indicates faults with a clear color coding. An electrician can immediately see if a channel is broken or shorted—no need to connect a laptop or open visualization software."

That visibility enables continuity. "Modules can also be hot-swapped without interrupting PLC operation… [and] replacement modules can plug directly into base units without any rewiring needed." For high-mix lines, those details reduce tool changes, cut waiting time, and turn a potential stop into a brief pause.

Connectivity Beyond Basic I/O

Modern workcells combine sensors, motion, and specialized devices—not just digital and analog I/O. "The ET200SP offers modules for IO-Link, CANbus, Modbus TCP, and other specialized protocols," Rajendra says. "We also provide technology modules for high-speed counting or positioning tasks [in] applications where the PLC scan time alone isn't fast enough."

By embedding protocol support for PROFINET, Ethernet/IP, and Modbus TCP directly in the I/O modules, the ET200SP eliminates the need for external gateways, reducing potential failure points and extending the same LED-based diagnostics to IO-Link and CANbus channels.

When it comes to safety, mixed architectures are standard practice. Rajendra describes how the ET200SP offers a practical way to simplify compliance and integration on complex stations: "Designers can mix fail-safe and standard I/Os in the same station, all connected to a fail-safe PLC." The result is one platform that spans sensor-rich inspection, motion-heavy assemblies, and specialty functions without swapping ecosystems or retraining the plant.

Built-In Security and Sustainability

Building security and sustainability into designs early is more effective than treating them as compliance checklists along the way. For platforms designed to be reused across machine generations, those decisions scale: deploy a secure, recyclable baseline once and replicate it fifty times.

"[Siemens] built PROFINET with Class 1 certification into the ET200SP, which prevents unauthorized configuration changes or firmware downloads," Rajendra explains. "Only trusted devices and software interact with the system." This security reduces change-control friction and hardens the path from commissioning through maintenance.

With sustainability, lifecycle matters as much as launch. Speaking on Siemens I/O modules, Rajendra states, "We design our [Siemens] hardware for recyclability under Ecotech standards," and he goes on to note that Siemens is "preparing for Europe's upcoming Cyber Resilience Act," which tightens security compliance by 2027. For manufacturers, those measures translate to fewer compliance gaps and a clearer audit trail—backed by infrastructure designed to be reused during upgrades and responsibly recycled at end-of-life.

Conclusion

The pattern is consistent: reuse a modular baseline, adapt each station, surface diagnostics where faults occur, and route operational data without disrupting control loops. That approach minimizes costs through design reusability, cuts downtime via channel-level visibility and hot-swap, and future-proofs connectivity through multi-protocol support.

Footprint pressure, connectivity demands, and sustainability expectations continue to grow. The Siemens SIMATIC ET200SP I/O modules meet those demands with compact hardware, flexible interface options—including copper or fiber—integrated diagnostics at the channel, and an ecosystem that grows with your application. For engineers, it's a practical way to design once, adapt often, and keep the line moving—without re-architecting whenever customer needs change. As Raj Rajendra of Siemens frames it, the goal is to help teams "save time, energy, and money."

Author

Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.



« Back


Siemens focuses on industry, transport, infrastructure, and healthcare and creates technology with purpose by adding real value for customers. Combining the real and digital worlds, this company empowers engineers to transform their industries and markets.


All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos