Honduras - Marcar Honduras

Confirme su elección de moneda:

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Collaborative Robots: Combining Machine Muscle with Human Dexterity Steven Keeping
While industrial robots dominate—as the best option for low-volume, high-mix assembly in mass-manufacturing—in comparison to human dexterity, a new generation of lightweight robots promises to marry the best of man and machine.

Using Logic to Understand Programmable Logic Devices Paul Golata
Like human minds, computing devices require logic to process information. Programmable logic devices (PLDs) follow a specific set of instructions to control, compute, store, manage, and manipulate electronic information. Several categories of PLDs exist, providing design flexibility.

Which Hardware in the Loop (HITL) Scenario Works for You? Bill Schweber
Hardware in the Loop (HITL) is the only practical way to test complex system hardware and software, and two ways of implementing it exist. Each approach has pros and cons, but in either case, developing the HITL installation can be a task as large as developing the system itself.

Making Mathematical Sense of PID Controllers Mike Parks
PID controllers are a popular method for including a feedback as a mechanism to help efficiently control industrial processes. Short for “proportional, integrative, derivative,” PID controllers keep the output of a system constant based on user provided setpoint. Tuning the PID controller parameters, though, requires a bit of math to maximize efficiency and minimize adjustments and corrections based on feedback.

Ladies & Gentlemen, Start Your (Pneumatic) Engines Bill Schweber
Electric motors may be the prime mover we think of first, but there are many applications that are better served by pneumatic motors driven by compressed air. These motors have very high torque even at low or zero rpm, and they’re also good for high-impact, low-repetition functions like driving large hammers or even forging presses. Of course, the absence of wiring and associated high voltages and currents make them explosion safe, user safe, and practical in wet environments as well.

Industrial Automation Marcel Consée
While the term „Internet of Things“ first turned up in 1985 (when the Internet as we know it today was not even a prospect yet), the need for an „industrial“ subset has been recognized only in the early 2000s. Today, Industrial IoT is being implemented far more rapid than a more generic IoT, and – believe it or not – the key drivers for that came out of Europe.

Developing Communications and Mapping for a New Generation of Driverless Cars Pedro Calomarde
A new generation of driverless vehicles is dramatically changing the way automotive systems are designed and built. These driverless car systems will have significantly increased communication capability, linking vehicles together on the road and back to the cloud. All of this will be controlled by high end processors with complex 3D mapping and control algorithms, and all of this needs to be made secure.

Autopilot vs. Autonomous Lynnette Reese
People have misperceptions about autonomy. Autopilots have been used in aircraft for decades. In newer planes and at properly equipped airports, the autopilot can also be used for landing, usually in dense fog with lots of radar equipment on the plane and on the ground, and the landing isn’t gentle. (Pilots occasionally perform a “greased in” landing, which is when touch down is so gentle you don’t even feel it. Be sure to congratulate your pilot if this ever happens.)

The Internet of Useful Things, or “The World’s Most Expensive Egg Timer” Lynnette Reese
How did we get here? I could use several lifetimes up just in projects. The tools available to the masses seem to be fueled by IoT. We can all engineer a little IoT, apparently.

Turn The Lights Down and Get Some REST: A Trojan Horse for Automating Commercial Buildings Mike Parks
At a recent energy conference there was a great deal of discussion on how the commercial real estate market might leverage the current infatuation with smart devices, and buzz around the Internet of Things to help propel building automation technology into widespread adoption. It would seem that the technology maturity, price points, and market desire are finally beginning to intersect. In the final analysis many experts, including technologists, energy managers, engineers, and real estate professionals seemed to converge on the notion that lighting will be the key technology that will help other control technologies, such as HVAC, to finally gain greater adoption rates.

All Authors

Mostrar más Mostrar más
Ver mensajes por fecha

Archivos